Hi all,
From my customer a question popped up concerning the USB0 interface on the OMAP L138 (OMAPL138BZWT4).
It is currently used throughout numerous projects at , as it is a part of their , an in house developed software platform based on the OMAPL138, and they have the following questions:
- "What are the consequences if the pin USB0_VDDA12 is not connected?"
- "It is not clear to us what “proper device operation” - as mentioned in the datasheet- means in this case?"
Thanks in advance,
Kind regards,
Louka