This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x Starter kit BOOT problem

Hi friends,

            I am new for this platform and Looking for your Guidances !!..

   I start working on AM335x_starter_kit. I am able to boot Kit with uSD-card which I got  with Starter kit, but when

   I prepare new uSD-card using pre-build  images which I got with Development kit by running using "create-sdcard" script. I am not able to boot board with this card. Getting below message.


Using SDKv05.05.

In uSD-card Boot partition MLO, uImage,u-boot.img are present

In uSD-card root partition root file system is present.

But while inserting it on board it is not responding. Only "ccccccccccc"  string is appears.

///////////////////////////// MSG on MINICOM/////////////////////////////////////////////////////////////////

Welcome to minicom 2.5

OPTIONS: I18n
Compiled on May  2 2011, 00:39:27.
Port /dev/ttyUSB1

Press CTRL-A Z for help on special keys                 
                                                        
CCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCC

////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

Regards

Vishal Rana

  • Vishal,

    The CCCCCCCCC output in the serial console means that no boot source was found and the board is waiting to boot from UART. The only reason for this I can think of is that something is wrong with your SD card.

    Do you run the create-sdcard.sh script with sudo from withing the <sdk_dir>/bin/ folder? Does everything complete correctly with no error messages?

    I know I suggested this in your other thread about the AM335x GP EVM, but can you try with a different SD card?

    Have you tried with a later version of the SDK? Version 05.05.00.00 is very old and I'm not familiar with its problems.

    Best regards,
    Miroslav

  • hi Miroslav,

         I tried same with other card also but fail to get any thing on minicom.

         One more thing I observe when I am running "setup.sh" after creating SD card using

         given script. I am getting following message


    /////////////////////////////////////////////////////MSG///////////////////////////////////////////////////////////////////////////

    -------------------------------------------------------------------------------
    This step will set up the u-boot variables for booting the EVM.
    Becuase the not all AM335x devices have a NAND, the u-boot variables will
    be stored in uEnv.txt on the boot partition. U-boot will read this
    file on boot.

    Autodetected the following ip address of your host, correct it if necessary
    [ 10.217.16.117 ]

    Select Linux kernel location:
     1: TFTP
     2: SD card

    [ 1 ] 2

    Select root file system location:
     1: NFS
     2: SD card

    [ 1 ] 2


    This SDK supports both the AM335x EVM and the BeagleBone/EVM-SK.
    A BeagleBone/EVM-SK has been detected as attached to your host system
    Are you wanting to configure u-boot for this device?  An
    answer of 'n' will configure u-boot for the AM335x EVM instead
    (y/n) y
    The boot partition doesn't appear to be mounted on the host.
    If you're using a virtual machine, please ensure it has been imported to Linux
    Please ensure the boot partition is mounted and run setup.sh again.
    Press Enter to exit
    ////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

    I am using Physically install ubuntu on my machine.

    Please help me because from Last month I am stuck in this only and this may effect me in my office.

    Regards

    Vishal Rana