This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C write1 failed with error 16 Device or resource busy

Hello

i have the error 16 on each  write sequence when doing this code :

  
    if ((dev_i2c = open("/dev/i2c-2",O_RDWR)) < 0) {
        printf("Failed to open the bus with error %d %s\n",errno,strerror(errno));
       /* ERROR HANDLING; you can check errno to see what went wrong */
        return;
    }

    // send out the seven bit address of the device followed by a read/write bit. The bit is set to 0 for writes and 1 for reads.
    if (ioctl(dev_i2c,I2C_SLAVE,I2C_EEPROM_UCR_ADDRESS) < 0) {
         printf("Failed to acquire bus access and/or talk to slave 0xAE with error %d %s\n",errno,strerror(errno));
        /* ERROR HANDLING; you can check errno to see what went wrong */
    }

    //write test sequence
    printf("write test sequence\n");
    // Set address
    eepromAddr = I2C_EEPROM_WRITE_ADDRESS;
     //eepromAddr = I2C_EEPROM_READ_ADDRESS;
    i2c_ptr[3] = (offsetAddr) & 0xAA;
     i2c_ptr[2] = (offsetAddr) & 0xFF;
     i2c_ptr[1] = (offsetAddr>>8) & 0xFF;
     i2c_ptr[0] = eepromAddr;
     if(write(dev_i2c, i2c_ptr, 4) != 1) {
         printf("I2C write1 failed with error %d %s\n",errno,strerror(errno));
     }

reading is OK with this code :

        printf("read test sequence\n");
         // Set address
     eepromAddr = I2C_EEPROM_READ_ADDRESS;
     i2c_ptr[0] = eepromAddr;
     if(write(dev_i2c, i2c_ptr, 1) != 1) {
         printf("I2C write failed\n");
     }
      i2c_ptr[1] = (offsetAddr) & 0xFF;
     i2c_ptr[0] = (offsetAddr>>8) & 0xFF;
     if(write(dev_i2c, i2c_ptr, 2) != 2) {
         printf("I2C write failed\n");
     }

     // Read 4 bytes from device
     bytesToRead=I2C_NB_BYTES_TO_READ;
     bytesRead = read(dev_i2c, &i2c_buffer[0], bytesToRead);
     if(bytesRead != bytesToRead)
     {
         printf("I2C read failed with error %d %s; nb of bytes read=%d\n",errno,strerror(errno), bytesRead);
     }
     else
     {
         for (i=0;i<bytesRead;i++)
             printf("byte read = %x\n", i2c_buffer[i]);
     }

my device responds on i2c2 with :~# i2cdetect -r 2  with address 57 (an M24128 device)                                             

#define I2C_EEPROM_UCR_ADDRESS       0x57
#define I2C_EEPROM_READ_ADDRESS      ( (I2C_EEPROM_UCR_ADDRESS <<1)|0x01)
#define I2C_EEPROM_WRITE_ADDRESS      (I2C_EEPROM_UCR_ADDRESS <<1)

have you any idea ?

thanks

regards