This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

After I convert BIOS 5 tcf to SYS/BIOS cfg file, compiling error

Other Parts Discussed in Thread: SYSBIOS

Hi 

I had convert my BIOS 5 *.tcf files into cfg file, and then I compile the project. It has following error.

Can anyone help me with that?

Thank YOu.

Xining Yu

**** Build of configuration Debug for project C6678 ****

"C:\\Program Files (x86)\\ccsv5\\utils\\bin\\gmake" -k all
subdir_rules.mk:17: warning: overriding commands for target `configPkg/linker.cmd'
subdir_rules.mk:7: warning: ignoring old commands for target `configPkg/linker.cmd'
making ../src/sysbios/sysbios.lib ...
cle66 C:/ti/bios_6_33_06_50/packages/ti/sysbios/BIOS.c ...
asme66 C:/ti/bios_6_33_06_50/packages/ti/sysbios/family/c64p/Hwi_disp_always.s64P ...
asme66 C:/ti/bios_6_33_06_50/packages/ti/sysbios/family/c64p/Hwi_asm.s62 ...
asme66 C:/ti/bios_6_33_06_50/packages/ti/sysbios/family/c64p/Hwi_asm_switch.s62 ...
asme66 C:/ti/bios_6_33_06_50/packages/ti/sysbios/family/c64p/Clobber_asm.s62 ...
asme66 C:/ti/bios_6_33_06_50/packages/ti/sysbios/family/c64p/Exception_asm.s64P ...
asme66 C:/ti/bios_6_33_06_50/packages/ti/sysbios/family/c64p/MemoryProtect_asm.s64P ...
asme66 C:/ti/bios_6_33_06_50/packages/ti/sysbios/family/c62/TaskSupport_asm.s62 ...
asme66 C:/ti/bios_6_33_06_50/packages/ti/sysbios/timers/timer64/Timer_asm.s64P ...
asme66 C:/ti/bios_6_33_06_50/packages/ti/sysbios/timers/dmtimer/Timer_asm.s64P ...
are66 BIOS.obj c64p_Hwi_disp_always.obj c64p_Hwi_asm.obj c64p_Hwi_asm_switch.obj c64p_Clobber_asm.obj c64p_Exception_asm.obj c64p_MemoryProtect_asm.obj c62_TaskSupport_asm.obj timer64_Timer_asm.obj dmtimer_Timer_asm.obj ...
'Building file: ../app.cfg'
'Invoking: XDCtools'
"C:/Program Files (x86)/xdctools_3_25_03_72/xs" --xdcpath="C:/ti/bios_6_33_06_50/packages;C:/Program Files (x86)/ccsv5/ccs_base;C:/ti/pdk_C6678_1_1_2_5/packages;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C66 -p ti.platforms.evm6678 -r debug -c "C:/Program Files (x86)/ccsv5/tools/compiler/c6000_7.4.4" --tcf --compileOptions "-g --optimize_with_debug" "../app.cfg"
xdc.tools.configuro: unknown option: --tcf
Usage: xs xdc.tools.configuro [--help]
[-v | -q]
[-@ optionsfile]
[-o outdir]
[-b config_bld | -c codegen_dir | --cb]
[-t target] [-p platform[:instance]] [-r profile]
[-Dname=value]
[-w | -x regexp]
[--rtsName pkg_name]
[--cfgArgs args_string]
[--linkTemplate linker_template]
[--pkg] [--generationOnly]
[--compileOptions compile_options_string]
[--oc compiler.opt] [--ol linker.cmd]
infile.cfg
js: "C:/Program Files (x86)/xdctools_3_25_03_72/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: fatal error
gmake: *** [configPkg/linker.cmd] Error 1
gmake: Target `all' not remade because of errors.

**** Build Finished ****

  • Xining Yu,
    check Project Properties->CCS Build->XDCtools->Advanced Options. There is an option "Read infile.tcf ...", which you should uncheck. That option should not be visible, so thanks for reminding us of that oversight.

    Also, I noticed that you installed XDCtools in a directory with white spaces in the path. Sometimes that causes various problems, so you may want to try installing XDCtools in a different directory if there are any further problems during the build.