Other Parts Discussed in Thread: SPRC133
Is there a CSL example showing working Isochronous USB communication? I have an application where I need two isochronous IN endpoints with a rather large payload (375 to 500 bytes). The C55x USB sample code that I have only has partial isochronous source code which is incomplete and commented out. Has anyone successfully used the CSL USB support for Full Speed bandwidth isochronous data transfer?