This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to double the refresh rate in DDR2 Controller when DDR2 memory is operating over extended temperature range?

Hi, 

  According to samsung or other DDR datasheet, At 85 - 95 °C operation temperature range, doubling refresh commands in frequency to a 32ms period ( tREFI=3.9 us ) is required, and to enter to self refresh mode at this temperature range, an EMRS command is required to change internal refresh rate.

   How to do that for dm365? Thanks!