Hi,
I have bought and installed C5505 USB stick and run few sample programs. These are the sample programs given in ccsv4\emulation\boards\usbstk5505\demo\USB_Stick_Sample\src (here programs use the register values directly without any API) and ccsv4\emulation\boards\usbstk5505\tests (here programs use non CSL APIs).
I downloaded the CSL (Chip Support Libraries) for C5505 (TMS320VC55XCSL-LOWPWR). It contained one executable which when executed created a directory with source and examples.
I imported and tried to run the examples. I am getting following error:
cannot find file "Debug/cslVC5505.lib"
This file cslVC5505.lib in my case is not getting created in Debug folder.
I would be glad if somebody responds and provides help.
(I read posts in the past regarding this error but could not figure out what exactly to change.)
Thanks.
Regards,
Vijay