Other Parts Discussed in Thread: AM3358
Hi
I am using the am3358.My board has a nand.I find a problem .
When the SD is in the board, i use the command of setenv and saveenv.But the environment variable is not save the nand.After the system is reset,the environment variable is not in the nand.
When the SD is out of the board.The command of setenv and saveenv is valid.The environment variable is save the nand.
I use the command of printenv,
U-Boot# printenv
autoload=yes
baudrate=115200
bootargs=console=ttyO0,115200n8 noinitrd ip=off mem=256M rootwait=1 rw ubi.mtd=7,2048 rootfstype=ubifs root=ubi0:rootfs init=/linuxrc
bootargs_defaults=setenv bootargs console=${console} ${optargs}
bootcmd=if mmc rescan; then echo SD/MMC found on device ${mmc_dev};if run loadbootenv; then echo Loaded environment from ${bootenv};run importbootenv;fi;if test -n $uenvcmd; then echo Running uenvcmd ...;run uenvcmd;fi;if run mmc_load_uimage; then run mmc_args;bootm ${kloadaddr};fi;fi;run nand_boot;
bootdelay=3
bootenv=uEnv.txt
bootfile=uImage
console=ttyO0,115200n8
ethact=cpsw
ethaddr=20:cd:39:d9:84:38
importbootenv=echo Importing environment from mmc ...; env import -t $loadaddr $filesize
ip_method=none
kloadaddr=0x80007fc0
loadaddr=0x82000000
loadbootenv=fatload mmc ${mmc_dev} ${loadaddr} ${bootenv}
mmc_args=run bootargs_defaults;setenv bootargs ${bootargs} root=${mmc_root} rootfstype=${mmc_root_fs_type} ip=${ip_method}
mmc_boot=run mmc_args; run mmc_load_uimage; bootm ${kloadaddr}
mmc_dev=0
mmc_load_uimage=fatload mmc ${mmc_dev} ${kloadaddr} ${bootfile}
mmc_root=/dev/mmcblk0p2 rw
mmc_root_fs_type=ext3 rootwait
nand_args=run bootargs_defaults;setenv bootargs ${bootargs} root=${nand_root} noinitrd rootfstype=${nand_root_fs_type} ip=${ip_method}
nand_boot=echo Booting from nand ...; run nand_args; nandecc hw 2; nand read.i ${kloadaddr} ${nand_src_addr} ${nand_img_siz}; bootm ${kloadaddr}
nand_img_siz=0x500000
nand_root=ubi0:rootfs rw ubi.mtd=7,2048
nand_root_fs_type=ubifs rootwait=1
nand_src_addr=0x280000
net_args=run bootargs_defaults;setenv bootargs ${bootargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp
net_boot=echo Booting from network ...; setenv autoload no; dhcp; tftp ${kloadaddr} ${bootfile}; run net_args; bootm ${kloadaddr}
nfsopts=nolock
nor_args=run bootargs_defaults;setenv bootargs ${bootargs} root={nor_root} rootfstype=${nor_root_fs_type} ip=${ip_method}
nor_boot=echo Booting from NOR ...; run nor_args; cp.b ${0x08080000} ${kloadaddr} ${nor_img_siz}; bootm ${kloadaddr}
nor_img_siz=0x280000
nor_root=/dev/mtdblock3 rw
nor_root_fs_type=jffs2
nor_src_addr=0x08080000
rootpath=/export/rootfs
script_addr=0x81900000
spi_args=run bootargs_defaults;setenv bootargs ${bootargs} root=${spi_root} rootfstype=${spi_root_fs_type} ip=${ip_method}
spi_boot=echo Booting from spi ...; run spi_args; sf probe ${spi_bus_no}:0; sf read ${kloadaddr} ${spi_src_addr} ${spi_img_siz}; bootm ${kloadaddr}
spi_bus_no=0
spi_img_siz=0x380000
spi_root=/dev/mtdblock4 rw
spi_root_fs_type=jffs2
spi_src_addr=0x62000
static_ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off
stderr=serial
stdin=serial
stdout=serial
Environment size: 2799/8188 bytes
Can you help me.