HI,
I am porting the Android ICS 4.0.3 to the Beagle Board. When I am booting the kernel from the SD card, It is giving the following error. So could you please help me on this.
usb 1-2.1: new high speed USB device using ehci-omap and address 3
usb 1-2.1: New USB device found, idVendor=0424, idProduct=ec00
usb 1-2.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
smsc95xx v1.0.4
smsc95xx 1-2.1:1.0: usb0: register 'smsc95xx' at usb-ehci-omap.0-2.1, smsc95xx USB 2.0 Ethernet, d2:1c:91:02:ce:5c
EXT4-fs (mmcblk0p2): recovery complete
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
VFS: Mounted root (ext4 filesystem) on device 179:2.
Freeing init memory: 216K
init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
init: cannot open '/initlogo.rle'
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
enabling adb
adb_open
root@android:/ # init: untracked pid 1007 exited
warning: `zygote' uses 32-bit capabilities (legacy support in use)
request_suspend_state: wakeup (3->0) at 16510101320 (2000-01-01 00:00:12.812072754 UTC)