Other Parts Discussed in Thread: OMAP3503
Hi,
We are using the camera to capture the video images. The captured image is streamed live onto LCD using a V4L2 test application. The following are the details
- OMAP3503 platform
- Camera with resolution 640x480 in VGA mode
- LCD with display resolution 800x480
- Linux 2.6.29 Kernel used
- Image format on camera side YUV 422
We are facing the problem of image not properly displayed on the LCD. The image has three part vertically
- First portion is proper
- Second portion should be prior to first portion but being displayed after first portion for few vertical lines
- Third portion has the repition of the last vertical line of second portion for few vertical ines
Please let me know if anybody else has faced similar problem and the work around/suggestions for the same
Thanks and Regards,
Srikanth