Other Parts Discussed in Thread: TVP7002, TVP5147
I saw "Luma or composite cable must not be plugout or plugin while streaming is going on. Otherwise, a split image will be captured " from SPRUG99A.pdf
Is there any patch about it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am afraid, re-synchronization is outside the scope of VPIF specification; therefore this is more of a hadrware limitation than a bug in the software driver.
That said, we have seen some users uses the I2C Sync Detect Status register on TVP5147 or TVP7002 to implement a polling mecahnism and detect when sych has been lost (disable VPIF) and when synch has recovered (enable VPIF) to work-around this issue.
look at the following App Note for a workaround: http://focus.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=sprab77
No, I follow sprab77 document - according to the example in this document once the sync is lost, the LSB bit in VPIF_CHO_CTRL register is set to 0 and as soon as the sync is detected, the same bit is set to 1.
Anyway, I also tried resetting after reconnect (i.e. when sync is lost, just wait for detecting it again and after detecting it, set the bit to 0 and then set it to 1), but this didn't help and I still get the split image.
Found the problem.
TI's solution works OK. The problem was that I use different video decoder from the one on the EVM and the registers which I checked in this decoder tell only if video signal is present on the input but cannot tell if the decoder actually outputs video data. Intorducing a delay after checking these registers (as a workaround) and then setting the LSB of VPIF_CH0_CTRL to 1 solves the issue.
FYI, sprab77 worked for me as well. I was taking two NTSC inputs from two TVP5147's. I wrote a combo function that checked both/either with the same loop. Also, note that I'm using dvsdk_3_10_00_11 and the code examples in sprab77 were TOTALLY INVALID, at least it seemed that way to me. Nevertheless, with the implied advice I was able to figure out how to do it. I modified the TVP5147 driver to have a function tvp514x_checkNTSClock that checked strictly for the lock on an NTSC signal. The caller to this function [messily] used a global that I made tvp514x_probe set, for the address of the v4l2_subdev, based on matched I2C address. The caller was board-dm646x-evm.c where I wrote a function that was called from an ioctl I had developed earlier.
This link is broken, please re-issue.Juan Gonzales said:look at the following App Note for a workaround: http://focus.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=sprab77
This post is old, but it seems people are still experiencing this issue. I wanted to post the link again, since as Mike stated, that link it broken.
http://www.ti.com/lit/an/sprab77a/sprab77a.pdf
Thanks,
Derek