This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352 MCASP0 pinmux violation

Other Parts Discussed in Thread: TLV320AIC3100

Hello,

I'm busy with the pinmux utility for Sitara Linux SDK 7.0 and I have configure some signals, but when I have configure them I get IO Set Violation.

MCASP0 I will use for an audio codec(TLV320AIC3100) and have used the following pins:

T5. MCASP0_AHCLKX -> AUD_MCLK

A13: MCASP0_ACLKX -> AUD_BCLK

B13: MCASP0_FSX -> AUD_WCLK

D12: MCASP0_AXR0 -> AUD_DIN

C12: MCASP0_AXR2 -> AUD_DOUT

A14, B12, C13, D13 are used for MCASP1

I have include the .dat file.

Thanks in advance

PinMuxDesignState_AM335x Rev 2.x.dat