This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WiFi-Direct/P2P Mode does not work on OMAP5432 EVM with GLSDK 6.04.00.02

Hi,

I find that the P2P/WiFi-Direct configuration commands (given via wpa_cli) do not work with the latest GLSDK on OMAP5432 EVM. 

root@omap5-evm:~# wpa_supplicant -Dnl80211 -c SHARED/wpa.conf -i wlan0 -B
Successfully initialized wpa_supplicant
rfkill: Cannot open RFKILL control device
[  109.003570] wlcore: PHY firmware version: Rev 8.2.0.0.195
[  109.108154] wlcore: firmware booted (Rev 8.8.0.0.13)
root@omap5-evm:~#
root@omap5-evm:~# wpa_cli
wpa_cli v2.0-devel
Copyright (c) 2004-2012, Jouni Malinen <j@w1.fi> and contributors

This software may be distributed under the terms of the BSD license.
See README for more details.


Selected interface 'wlan0'

Interactive mode

> p2p_find
FAIL

Scanning & connecting to a regular Access Point goes through fine without any issues. 

Can you let me know if a fix for this issue is imminent ? This used to work with GLSDK 6.03.

Thanks,

Anurag Maheshwari