Other Parts Discussed in Thread: TMS320C6748
Hello,
I've recently been having an issue with excessive current draw from the TMS320C6748 DSP. In some cases, the device will power up correctly and the total current draw for the system is 1.55 A. However, it will also power up in a different state, where the current draw for the system is 2.35 A. I have checked the current draw on different rails and it is clear that the 3.3 V supply is drawing the excess current. The device has operated as expected in the past in both states, so I was wondering if there could be a configuration issue with the DSP or if it is more likely that the chip has been compromised. I have also noticed that in recent testing the output voltage on the 3.3 V line is being pulled low (to ~2.98 V) and the 1.8 V connected to the DSP is being pulled high (~2.6 V). While this is happening, the DSP is no longer operating correctly. The initial design did not have a power monitor circuit to hold the DSP in RESET until power was good on all 3 rails, so that has been implemented more recently, but the same behavior persists. Is there something that I'm missing that would cause a soft short between these rails? Also, what happens to the DSP if a FPGA tries to send data across while it is in RESET (this shouldn't be happening, but I'm curious as to the result)?
Thanks