Other Parts Discussed in Thread: OMAPL138
i am using edma to store incoming rx chars from uart 2 in L2 SRAM. i am using a "bare metal" DSP application.
the uart baudrate is 460 kbaud, so 14-byte packets arrive in about 1/3 msec. I have confirmed this using a scope.
The edma stores the incoming data correctly, but it takes several msec to do so -- i poll the dma index register CCNT periodically, so i can monitor the data transfer.
Is the latency in the uart, or the dma? is there any way to fix this?