Hi,
I read that SRIO in 6678 can be configured for 4 x 1 and 1 x mode.
So i would like to configure as follows.
DSP ---lane0----------------- Device 1
-- lane1 ----------------- Device 2
-- lane2 ----------------- Device 3
-- lane3 ----------------- Device 4
each laneX(x=0,1,2,3) is different rate setting.(5G, 3.125, 2G , 1G)
Is this configuration possible ?
And the answer is same for 66AK2Hx ?
EmbeddedHolic.