This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What is the configuration file and target for building meta-arago to reproduce the exactly same result of ti-sdk-am335x-evm-06.00.00.00?

Hi

I'm trying to build meta-arago according to the explanation of arago-project.org.

I used the following configuration and build target

./oe-layertool-setup.sh -f ./configs/amsdk/amsdk-06.00.00.00-config.txt

MACHINE=am335x-evm bitbake arago-core-tisdk-image

According to http://arago-project.org/wiki/index.php/Setting_Up_Build_Environment, the above build target - arago-core-tidsk-image - must be the most complete one.

I think, it means that this target will produce the most fully containing result. Right?

But the resultant fully containing root filesystem - tisdk-rootfs-image-am335x-evm-20140522045357.rootfs.tar.gz - is slightly different from the one provided by ti-sdk-am335x-evm-06.00.00.00.

The rootfs provided by ti-sdk-am335x-evm-06.00.00.00 contains more binaries than the one of my own build

(the small version of rootfs - arago-base-tisdk-image-am335x-evm-20140522045357.rootfs.tar.gz is the same as the one provided by  ti-sdk-am335x-evm-06.00.00.00)

I wonder if I used correct bitbake target.

So, My question is..

What is the configuration file and target for building meta-arago to reproduce the exactly same result of ti-sdk-am335x-evm-06.00.00.00?