Other Parts Discussed in Thread: SYSBIOS, CCSTUDIO
Hello,
Im implementing an ARM-DSP communication using IPC based MessageQ.
When I load and run the DSPs the next message in the /remoteproc0/trace0 appears:
VirtQueue_init(): MultiProc_self already set!
The program nor even start the main from the .c file. It seems to be a configuration file issue, but I had changed many things in the .cfg file but this still appears.
This was just if I want to run the DSPs, therefore when I try it with the ARM side, I think as the DSPs are not initializated well, IPC_start() fails and the application never runs as expected
Does anyone know why is this problem?
Thank you
Ronny