This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDR3 512M



Hi all,

I am trying to activate the second half of my DDR3 memory.  It works just fine if I use the default memory size of 256M.  I can run the memsize command and it stops at 256M as expected.

If I modify the uBoot boot args to have mem=512M and rerun the memsize command the kernel oopses.

Where should I look for the issue?

Chuck

root@am335x-evm:~# mem
memInfo.sh  mem_util    memsize     
root@am335x-evm:~# memsize
[   30.772792] ------------[ cut here ]------------
[   30.777717] kernel BUG at mm/slab.c:501!
[   30.781867] Internal error: Oops - undefined instruction: 0 [#1] PREEMPT