Out of our Camera: 1080p30 YcBcR
A 30 Hz Frame rate, over a 20 Bit BUS consisting of:
· 66Mhz Clock
· 16 Bit Video BUS
· HSYNC
· SYNC
· DE
This signal has shortend the blanking. That’s how they clock the data out at a slower rate.
The Cameras 66MHZ SMPTE274, 16 bit signal; has a blanking of 66288
We want to output to match the SMTPE 274M standard (1080p30)
Add the Blanking and reclock the data at 74.25 MHZ clock
16 Bit Video BUS
HSYNC data rate stays the same.
VSYNC stays the same (30Hz)
DE
Note: The 274M spec is 2200 pixels x 1125 lines = 2,475,000 samples per frame.