I'm considering a new design using the AM3359. I currently use the TMS320F28xxx series with CCS5 and a XDS510PP pod for all of development.To get a handle of what's needed, I've installed the ARM compiler in CCS5 and in starting a new project, the only choice for a device close to the AM3359 is "generic cortex A8". Is this the best/correct choice for this device, or do I need additional software?
Also, the TMDSICE3359 communications engine make reference to a USB emulator built into the board. To run this board with CCS5 do I just need a USB connection to the board with no other hardware (pod)? Will my 510PP pod work with this EVM if I adapt to the 20-pin JTAG header?
(The whole tools section for these parts is pretty sparse/convoluted with lots of circular references on the wiki's. There should be a table that shows what's needed for software and hardware for development, keeping it simple).
Thanks.