Hello,Tier.
We have a case that DM8168 will be conncted with another DM8168 or C6678.Here we just talk about two DM8168's case.
1>Could the two DM8168 both boot with Nand-Flash boot mode?
if so,should we need to ensure that EP power up first,then RC power up?
2>In the following link:
http://processors.wiki.ti.com/index.php/TI81XX_PCIe_FAQs#How_can_I_initialize_PCIe_module_on_DM816x_to_be_used_as_PCIe_Endpoint_without_using_any_of_the_PCIe_Boot_mode.3F
How can I initialize PCIe module on DM816x to be used as PCIe Endpoint without using any of the PCIe Boot mode?
It says that we need to program some registers for the EP could work normally.However,if we design a product with two Dm8168 connected with PCIe,it can not be so.Then,we need to modify the Uboot to perform the programming operation?
Or,just ensure the DM8168 EP power up completely,and then power up DM8168 RC.So,the EP can be detected by RC.Is it OK?
BR!