I am using TI AM335x processor on the TI package am335x-evm-sdk-src-07.00.00.00.tar.gz and kernel linux-3.12.10-ti2013.12.01
In the kernel DeviceTree, I set GPIO1_14 (multiplexed with pr1_pru0_pru_r31_14) as
(PIN_INPUT_PULLUP | MODE7)
We let this pin as input floating, it should be pulled up by internal resistor, but when we read the value by using
cat /sys/class/gpio/gpio46/value
we get 0 "Low",
Only if we input 1(high) externally, we get 1 "high".
What's wrong with it?
Thanks!