This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Development board for OMAP3xxx

Hi,

I am looking for development board that can run full Android and Linux including UI.

The purpose of the board is to develop, test and evaluate Siano TV tuner chip connected to TI processor.

The chip can to work with I2C, SPI and/or SDIO. Not at the same time, but since we support all 3 interfaces we would like to test all on same board.

BeagleBone black seems to be a good choice but it is not available anywhere.

Another option we were offered is tmdssk3358 from TI, but it doesn't have SDIO access on any of the expansion connectors, and the only available SDIO bus is used for boot which means we can't use it.

Any other suggestions?

Requirements are: Can run Android and Linux (and has an open source of working solution available)and has expansion connector with access to available SDIO, SPI and I2C busses 

Thanks,

Doron Cohen