This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3 WinCE 6.0 BSP 4-bit mode Support in SDIO Driver

All,

We are trying to integrate a Murata WL8686 WLAN Driver into the 6.12.03 version of the OMAP3 WinCE BSP.

For some reasons, we are seeing that the SDIO Card times out waiting for the interrupt in Window CE. On 1-bit mode, the WLAN Card works correctly but the throughput is no where near the requirement. When we switch to 4-bit mode, the WLAN card time-outs and does not complete initialization.However the driver in Linux is functional normally.

Is there any limitations with the SDHC Driver provided with the BSP for supporting SDIO Devices [like Wi-Fi, Bluetooth] in 4-bit mode. What kind of SDIO validation has been done on this Driver?

Please let us know.

Thanks,