This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flashing TI ICE 3359 using SPI

Hello,

I am using TI ICE 3359 for one of my university project and this is my first hands on with TI device. 

I am using Ubuntu13.10 64bit OS and downloaded the "ti-sdk-am335x-evm-07.00.00.00" for testing some arm benchmarks in it. 

i wish to flash my application using the SPI flash and installed "AM335X_StarterWare_02_00_01_01" assuming it is the flashing tool.

But in the wiki page it states to start with ccs and load the gel file. I am CCS and i have example application build with the above sdk. I wish to flash those files and test it.

I am not able to understand the way to flash using SPI as i am not using CCS (CCS had some problems with ubuntu13.10 as it was 32bit and could not install).

Can someone guide me how to use this StarterWare to load the files into target.