Hi,
I am a newbie of EVMK2H.
The board version is 3.0
I have programmed the keystone-evm-ubifs.ubi to nand and linux boots OK.
and as says in quick start datasheet , there is web page to test arm/llinux functions.
Now i have some questions.
1. How to program DSP ?
If DSP is accessed via JTAG, linux may can not run.(I thinks share same jtags scan).
How can DSP be programmed whilest arm is running linux ?
Or other method ?
2. I want to send packet to DSP and DSP return.
Which example or manual could be help for me?
3. Finally i wanna setup as follows.
packets are traversing :
PC--->ARM(utilize muliple core, linux) --> DSPn ->DSPm -> ARM ---> PC
where is should start ?
EmbedHolic