This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVMK2H ARM and DSP configuration possible ?



Hi,

In datasheets, there are two boot mode via DIP switch

A. boot

B. no boot

Case A,

Arm is booting  linux normally, which mode DSP is in this case ?

Is it possible to boot DSP ?

Case B,

How to boot ARM with linux ?

ARM and DSP are run program  from JTAG ?

In above two case, is it possible that ARM is in little-endian and DSP is in big-endian ?

EmbedHolic