Hi everyone,
I'm very interested in running a linux on c6678 DSP, so I found an old post to run a linux on EVM6678L board http://linux-c6x.org/wiki/index.php/Linux-c6x_2.0_Release . This release requires a 32-bit ubuntu 10.04, but I only have 64-bit 12.04 installed on my computer, so I used a virtual machine under VMWare workstation 10.0. I prepared the exact software tools according to the release (I used newer version on my 12.04, but it also turned out to be unhelpful). When I program the linux binary to the evm6678l board, the board cannot be connected, the error message is as follows:
flxInitLoad: client has not been protected.
flxInitLoad: client has not been protected.
SEVERE: IcePick_D: Error connecting to the target: (Error -151) @ 0 (0x0)
SEVERE: emulation failure occurred
SEVERE: Error connecting to the target: emulation failure occurred
I can recognize the emulator in VMWare, and I can also connected the board in host OS (12.04) with CCS(ccs5.4), but I cannot connect it in the virtual OS 10.04 even using CCS (ccs5.0.3).
Does anyone know what the reason to cause the error? Or do you know about an alternate option to run linux on the DSP, any links or docs would help a lot?
Thank you very much!
Jie