Other Parts Discussed in Thread: 4460, 4430
I have an OMAP4430 in a design for a device and need to understand the lifetime of the part. Table 3-4 lists Power On Hour Limits for the device, with the vast majority of the time being in a retention state, presumably analogous to a smart phone in standby. Note 1 on the table indicates that TI should be contacted for use cases different than this.
Our device may have the display running the majority, or conservatively all of the time, and need to understand how this may impact lifetime of the part. Will this part be able to support continually running a display, and if so does it change the 5 year life time?
I have also considered transitioning to the 4460 or 4470, would this impact the part's life time? This may be an option but it seams the parts are not pin compatible so staying with the 4430 is preferable.