The GPMC on the OMAP3530 is meant for interfacing to external memory such as NAND and NOR flash; this is the same purpose as the EMIF16 interface on the KeyStone I/II devices. Are the main differences between these interfaces documented anywhere? If not, what are the major differences that someone familiar with GPMC on OMAP3530 should be aware of when moving to a KeyStone part (in particular the K2E family)?