Hi,
Now I want to rebuild the kernel in GLSDK according to the note "http://processors.wiki.ti.com/index.php/OMAP5_GLSDK_Software_Developers_Guide#Building_Yocto_Filesystem".
But the develop guide do not include the method to do this.
As you know, I can use "build-speicific-recipe.sh omap5-evm -f -c menuconfig busybox" to configure busybox and then rebuild to prepare the ipk.
But kernel is image type, not ipk type.
So if someone can tell me the method to rebuild the kernel?
Thanks and regards,
Jianqiang Yan