I have been using TMS320C6711 to remove 50 hz frequency . But i am unable to reduce the sampling rate for it. as it is given that samplig frequency is fixed to 8000hz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have been using TMS320C6711 to remove 50 hz frequency . But i am unable to reduce the sampling rate for it. as it is given that samplig frequency is fixed to 8000hz
Hi,
Thanks for your post.
Please give us more details in elloborating your necessity to remove 50 Hz frequency. Are you using TI provided code or your own code?
Which TI software package are you using to run the code? Which application are you trying to develop to reduce the sampling rate?
Are you using custom board based out of C6711 TI board?
Kindly provide us all details to proceed further.
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
-------------------------------------------------------------------------------------------------------
Hi,
Kindly answer the following questions to address your issue in a better way:
Are you using TI provided code or your own code?
Which TI software package are you using to run the code?
Which application are you trying to develop to reduce the sampling rate?
Are you using custom board based out of C6711 TI board?
Thanks & regards,
Sivaraj K
-------------------------------------------------------------------------------------------------------
Please click the Verify Answer button on this post if it answers your question.
-------------------------------------------------------------------------------------------------------