Hello,
Could you give me Makefile of OpenSSL for AM3352 in SDK v7.0?
Now, I want to install OpenSSL v1.0.1g by shared object (.so) format (libssl.so.1.0.0 and libcrypto.so.1.0.0), because pre-installed OpenSSL v1.0.1e has the Heartbleed problem.
Therefore, I'm consulting the method described in the following URL to install OpenSSL v1.0.1g.
http://processors.wiki.ti.com/index.php/Build_OpenSSL_for_Sitara
However, the shared object (.so) is not build, because the configure command isn't be used (the "shared" option can't be used).
Now, I changed the Makefile a bit, and I can build the shared object file (libssl.so.1.0.0 and libcrypto.so.1.0.0).
However, the object file doesn't work correctly (it seems that Crypto Hardware Accelerators on AM3352 doesn't work).
I think my Makefile has some mistakes.
OpenSSL v1.0.1e in SDK v7.0 work correctly, and I think someone has a correct Makefile to build OpenSSL v1.0.1e using Crypto Hardware Accelerators on AM3352.
Therefore, I want to consult the correct Makefile.
Best Regards.
Nomoto