Hello
Yesterday, I just repeated what Sam had done (of this thread) last year.
http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/259301.aspx
First, I have created a SYS/BIOS (v6.4) project (as simple as a "hello" RTOS code, a Timer only) for LCDKOMAPL138's ARM core, and it worked just fine (with a Timer spinning correctly). This proved the backbone TI-RTOS was working. Then, I tried pulling in another known good StarterWare (1.10.04.01) 'gpio' sample project with some initialization functions sitting in the main(), prior to entering the BIOS_start(). The result is almost the same: my LCDKOMAPL138 crashes at the PSCModuleControl function, only at different address HWREG(0x01E27000 + offset).
1) Why SYSBIOS stop working once I add StarterWare? Is there any comment from TI or any pioneers? Thank you!
My guessing is that I should do some reconfiguration on RTOS’s .cfg file, but I do not see any problem about memory conflict like in a linker command file (no .cmd file anyway). As I tried to edit the .cfg file, I simply got two empty columns [Package Name and CPU Core]. I was not allowed to do any edit/view for .cfg reconfiguration. Thus, we could not trace how the system has crashed and we have no access to edit/view it.
2) How do I manage the .cfg file (or any .cmd if needed) for RTOS to work with StarterWare)?
Please help!
Thank you!
YeuShyr