This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CPU load graph in CCSv6 using DSP/BIOS 5.42

Good day experts,

I upgraded my CCSv5 today with CCSv6.

I am still using DSP/BIOS v5.42.01.09 for my applications and I would really like to display the CPU load graph as well as the LOGs. I tried to set this up in CCSv6 from the Tools -> RTOS Analyzer in the Debug perspective, but it requires some UIA configuration file, which I am unfamiliar with (I am assuming it has to do with SYS/BIOS).

Is CPU load graphs supported for DSP/BIOS v5.42.01.09 in CCSv6? If so, how can I set it up?

Thanks in advance!