Hello, is there any data related to the allowable error on the receive baud rate for the C5505's UART? We have the C5505 running at 2.048 Mbaud, and the device it is communicating with is 2 Mbaud.
I did notice datasheet table 5-31 "Timing Requirements for UART Receive", however these values seem very restrictive (bit width +3/-3.5 ns); especially restrictive for low baud rates. Is it possible the units on this table were supposed to be "%" instead of "ns"?
Thanks - AM