This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530 memory map mismatch

Hi All,

I'm new with the OMAP processor. I'm trying to run the scale example from the codec engine examples and I encounter with a mismath problem.

<1>DSP-side configuration mismatch/failure

DSP-side configuration mismatch/failure

<1>0 -> success

0 -> success

<1>Positive value -> DSP-side failure code.

Positive value -> DSP-side failure code.

<1>(Uint32) -1 -> DSP-side component was not initialized.

(Uint32) -1 -> DSP-side component was not initialized.

<1> ProcId received : 0, Expected : 0

ProcId received : 0, Expected : 0

<1> DRV configuration status [0x0]

DRV configuration status [0x0]

<1> IPS configuration status [0x0]

IPS configuration status [0x0]

<1> POOL configuration status [0x0]

POOL configuration status [0x0]

<1> MPCS configuration status [0x0]

MPCS configuration status [0x0]

<1> MPLIST configuration status [0x0]

MPLIST configuration status [0x0]

<1> MQT configuration status [0x0]

MQT configuration status [0x0]

<1> DATA configuration status [0xffffffff]

DATA configuration status [0xffffffff]

<1> RINGIO configuration status [0x0]

RINGIO configuration status [0x0]

app: error: can't open engine scale

I looked for the cause of the problem with the CE_DEBUG=2 option and I saw that there is an error (0x800008052  -DSP_ECONFIG).

I saw that the error is caused beacuse of a mismatch with the memory map between the  DSP & the GPP sides.

How can I know is the differnce between These two sides and how can I fix it (which files I need to align).

Regards

Eran