This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[C6747/DA8xx] IPU/IPD is valid during reset ?

Other Parts Discussed in Thread: DA8XX

Hi

I would like to confirm whether IPU/IPD registers are valid or not while reset pin is being asserted.
The same has been discussed here for OMAPL137.

http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/p/235970/831493.aspx#831493

I believe the same is also applicable for C6747/da8xx. Correct, right ?

Best Regards,
Kawada

  • Hi Kawada,

    Thanks for your post.

    Yes, you are correct, it should be applicable to c6747/da830 but not da8xx.

     IPU/IPD value will remain same and never change during and after reset.

    Thanks & regards,

    Sivaraj K

    -------------------------------------------------------------------------------------------------------

    Please click the Verify Answer button on this post if it answers your question.

    -------------------------------------------------------------------------------------------------------

  • Hi Sivaraj,

    Thank you for your reply. Great to know that!
    For further my understanding, it is good to know it is same to c6745/da808 also.

    Thanks.
    Kawada

     

  • Hi Kawada,

    Thanks for your update.

    It is not same for c6745/da808 since this is of different architecture.

    Thanks & regards,

    Sivaraj K

     

  • Hi Sivaraj

    Thanks for your update.
    My understanding is that c6745/da808 is almost same in HW point of view and these devices are based on primus (OMAPL137) architecture. So, if OMAPL137's IPU/IPD is valid during reset, I wondered the behavior of c6745/da808's IPU/IPD was also same with OMAPL137's one.
    Did you mean this understanding was not correct ?

    Best Regards,
    Kawada

  • Hi Kawada,

    Thanks for your update.

    You need to check both the schematics of c6747/DA830 & c6745/DA808 and confirm whether in HW point of view, if it is same and I agree that, both the devices are primus based. I didn't mean, your understanding is wrong, just you need to confirm, both the devices should be same in HW point of view. If it is so, c6747/OMAPL137's IPU/IPD would be valid during & after reset.

    Thanks & regards,
    Sivaraj K