This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTDX without DSP/Bios on DM6437?

Hi all,

i like to use RTDX to display small logging and debug messages from my EVM
DM6437 on PC. Using DSP/Bios, this works fine. But for my application it would
be better, if it worked standalone without OS. Is that possible at all?

I tried to follow the steps in spra895 -> 2.2 RTDX Without DSP/BIOS
and did the following:
- link rtdx.lib from bios_5_33_06\packages\ti\rtdx\lib\c6000\ to my project
- set up a interrupt vector table with IRQ 3 (offset 0x60) calling RTEMU_msg
- write the vector table address to ISTP register
- enable interrupts
- create an output channel and send an integer by calling RTDX_write().

I see, that RTEMU_msg() is called once after setting up interrupts.
When I load the program, the channel is detected by the Channel Verwer Control
and it gets active as RTDX_enableOutput() is passed. But no data is received by
CCS, the logfile remains empty.

Is DSP/Bios needed or could it work without and something is missing?

Thanks,
Tobias