This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Framebuffer display problem

Other Parts Discussed in Thread: TMS320DM6446

Hi,

I use an Angstrom kernel 2.6.32 build with openembedded on a DM6446 processor.

When I write an RGB565 bitmap image to the framebuffer (OSD0 layer) than the displayed

image is somehow distorted. You can see this especially in the text. It looks like if there is some

uncorrect offset when the driver displayes the second frame of the image.

 

I use the following bootparameters to initialize the framebuffer driver:

davincifb:vid0=0,2500K:vid1=720x576x16,2500K:osd0=720x576x16,2025K:osd1=720x576

 

The displaying of images works perfectly with an old Montavista kernel. I have looked for

specific driver options but didn't find nothing which did really help.  Any suggestions where I

could look or what could be wrong?

 

Thanks

Philip Oberstaller

 

Original image:

Displayed image: