Hello
I have a doubt about TMDXLCDK6748.I have read that this board has a camera connector, but it is only for leopard imaging cameras.
I want to build a system to do some image processing. I want to connect a CMOS sensor to the board, then I will save the pictures in the RAM and do the algorithm. I would like to know if it is possible to connect a CMOS sensor to this board using the GPIOS. I have seen that the board has an expansion port with the GPIOS.
Thank you very much
Kind Regards