I'm trying to understand better how the IP address is/should be assigned to the AM335x.
I have a Linksys Cisco router that's connected to our network and to my laptop. I used one of the ports on that and connected the AM335x board to it but didn't get an IP address.
When I checked the ifconfig there was only the loopback address present.
I checked out the boot arguments and it looked like ip was being set to ip_method, which is not set.
I thought I could set an address as such:
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait ip=169.254.0.2 consoleblank=0
And doing this, did get me an IP address, but not what I expected:
126.1.70.136 login: root
-sh-4.2# ifconfig
eth0 Link encap:Ethernet HWaddr D0:FF:50:2A:18:7C
inet addr:126.1.70.136 Bcast:126.1.70.255 Mask:255.255.255.0
my laptop (same router) is 126.1.70.83, and I was able to ping the board, so I know it worked to obtain the IP address... but it took a long time, and the IP was not what I had expected. Can I get advice on what went wrong and what would have worked to get my expected results?