This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Communication between Beagleboard-xm and LM3S8962

Other Parts Discussed in Thread: LM3S8962

Hi all.

I'm doing a project with Beagleboard-xm and I want to send data from BBXM to LM3S8962 board via I2C interface. I use TCA9406 as Voltage-Level translator. When I use "i2cset 1 60 0 80" command (i2c-1 bus, LM3S8962's address is 0x3c, data address 0x0a, data 0x50), sometimes it can write but sometimes has Error: Write failed (ratio is about 50%).

Does anyone know what the reason to cause the error?

Thank you very much!

  • Hi,

    This random behaviour may be due to some hardware issue. Check the signal cables. Do you use internal or external pull-up resistors on the I2C bus lines? Check this as well. Finally, if you have access to an oscilloscope or a logic analyser, you may try to check what is going on on the I2C bus.

    Best regards,
    Miroslav