Hello,
I use C5535. In the IDLE-mode the power consumption on DVDDIO is too high.
I have locate the problem at SPI_RX and SPI_TX pin. I think the Pins are floating because the
connected devices are high impedance.
If I pull-up this pins with 100k each, the power consumption is ok.
But this is not possible in my layout.
Can I turn off SPI or do something else in Software to reduce the power consumption in IDLE-mode.
Thanks and Regards