Hi,
I have two different revisions of AM335x EVM boards.
With one board(REV 1.1A), boot.bin which is generated from compiling AM335X_StarterWare_02_00_01_01-master code as BOOT mode set to UART is loaded succesfully and executed also. But other board(REV 1.4A) if i do the same, loaded successfully but not executed. Please some one help me on this.
Regards,
Bhimesh