Hi,
I am using TMS320TCi6482 DSP with SRIO as bootloader option. Our software use SRIO NWRITE_R operation to write to another processor (Power Quicc 3). I am using LSU register set 2 for this. Every 20 millisecond, 2 MB of data is pumped through SRIO towards PQ. There is a SRIO switch in between. Sometimes, during the run, I received SRIO error - "Transaction complete, packet not sent due to unsupported transaction type or invalid programming encoding for one or more LSU register fields". I have taken the hexdump of LSU registers but the values found to be correct. I have noticed one thing, though, that this error comes only when software has tried to write 3 bytes of data.
So far, I am not able to figure out the reason for this error. Please help me in finding the cause for this error.
Thanks.
Aradhana