This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM385 : unhandled exception in [m3vpss]

Other Parts Discussed in Thread: TPS65913

Hi, TI experters

I make custom board without TPS65913 from IPNC RDK Ver3.5.

The unhandled exception occur after “[m3vpss ]  5511: SCLR: Create Done !!!” at every booting time.

I had done SWL, and the result of mtest command in u-boot is OK in 3 days test.

What should I do?

 

Log message is belong.

 

[m3vpss ] {SWOSD} edma3Handle->tccVal = 36

 [m3vpss ] {SWOSD} edma3Handle->chId   = 36

 [m3vpss ] {SWOSD} edma3Handle->tccVal = 37

 [m3vpss ] {SWOSD} edma3Handle->chId   = 37

 [m3vpss ] {SWOSD} edma3Handle->tccVal = 38

 [m3vpss ] {SWOSD} edma3Handle->chId   = 38

 [m3vpss ]  5412: SWOSD   : Create Done !!!

 [m3vpss ]  5510: DUP   : Create Done !!!

 [m3vpss ]  5510: SCLR: Create in progress !!!

 [m3vpss ]  5515: SCLR    : Loading Up-scaling Co-effs ...

 [m3vpss ]  5515: SCLR    : Co-effs Loading ... DONE !!!

 [m3vpss ] SCLR:HEAPID:0        USED:64

 [m3vpss ] SCLR:HEAPID:1        USED:5952

 [m3vpss ]  5516: SCLR: Create Done !!!

 [m3vpss ] Unhandled Exception:

 [m3vpss ] Exception occurred in ThreadType_Task

 [m3vpss ] handle: 0x8e621380.

 [m3vpss ] stack base: 0x8eeab180.

 [m3vpss ] stack size: 0x8000.

 [m3vpss ] R0 = 0x481d6000  R8  = 0x8ddb7e58

 [m3vpss ] R1 = 0x481d6010  R9  = 0x8f213178

 [m3vpss ] R2 = 0x00000000  R10 = 0x8f21317c

 [m3vpss ] R3 = 0x8eeb3058  R11 = 0x8f213e50

 [m3vpss ] R4 = 0x8e6a2558  R12 = 0x8eeb301c

 [m3vpss ] R5 = 0x00000000  SP(R13) = 0x8eeb3038

 [m3vpss ] R6 = 0x00000001  LR(R14) = 0x8dde5479

 [m3vpss ] R7 = 0x00000000  PC(R15) = 0x8dd8694e

 [m3vpss ] PSR = 0xa1000000

 [m3vpss ] ICSR = 0x00400803

 [m3vpss ] MMFSR = 0x00

 [m3vpss ] BFSR = 0x82

 [m3vpss ] UFSR = 0x0000

 [m3vpss ] HFSR = 0x40000000

 [m3vpss ] DFSR = 0x00000000

 [m3vpss ] MMAR = 0x481d6010

 [m3vpss ] BFAR = 0x481d6010

 [m3vpss ] AFSR = 0x00000000

 [m3vpss ] Terminating Execution...

INIT: Entering runlevel: 5

 inside autorun

 sbulla: unknown partition table

 sbulla: unknown partition table

Starting telnet daemon.

Starting syslogd/klogd: done