This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Display parameters for different resolutions

I have to set the following for different display resolutions.

  1. HBP (Horizontal Back Porch)
  2. HFP (Horizontal Front Porch)
  3. HSW (Horizontal Sync Width)
  4. VBP (Vertical Back Porch)
  5. VFP (Vertical Front Porch)
  6. VSW (Vertical Sync Width)

I'm using the CEA-861-E standard for referring the values. As it is not available online, please refer to an older version - CEA-861-D standard 

http://blogimg.chinaunix.net/blog/upfile2/090903185737.pdf

I have the following doubts.

  1. The frames per second I'll have to use is 60. So, in Page 13 Table 2 Video Format Timings—Detailed Timing Information, I have check the rows mentioned as 60 Hz. Am I right?
  2. Only a few resolutions are mentioned under 60 Hz. Eg., 1920 x 1080. If I need to check the values for 1680 x 1050, 1440 x 900, etc. what should I do? (The HBP,HFP,etc. values are not mentioned in CEA-861-D standard document. But, are given in CEA-861-E standard document.)
  3. Does the 480p, 1080p mentioned based on the VActive value?