This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

yocto filesystem building error



Hi,

while building the yocto file system I got the following error:

cp cann't stat "/mnt/yocto/yocto_repo/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-3.8-oe-linux-gnueabi/external-linaro-toolchain/2013.03-r2-arago5/SUPPORTED" as SUPPORTED file was not there. I created a file named SUPPORTED, then it worked

Then the next error was as follow:

DEBUG: Python function sysroot_cleansstate finished
DEBUG: Executing shell function do_configure
/mnt/yocto/yocto_repo/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-3.8-oe-linux-gnueabi/zlib/1.2.7-r0/temp/run.do_configure.22508: 80: /mnt/yocto/yocto_repo/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-3.8-oe-linux-gnueabi/zlib/1.2.7-r0/temp/run.do_configure.22508: ./configure: not found
ERROR: Function failed: do_configure (see /mnt/yocto/yocto_repo/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-3.8-oe-linux-gnueabi/zlib/1.2.7-r0/temp/log.do_configure.22508 for further information)

please, reply fast